Ride for Habitat 2013

08/28/2013

Ride for Habitat 2013

PLEASE NOTE: This event has been postponed until next year.

Grundfos is proud to be a Platinum Sponsor of the 4th annual Ride for Habitat. The event encourages all motorcycle enthusiasts to ride out in support of Habitat for Humanity and help provide low income families with affordable housing.

Don’t ride? No problem! You can still support by pledging to the riders registered for the event. 100% of all donations will go to help build Habitat homes.

Register or donate at: www.rideforhabitat.com

The event includes four starting points/routes for participant convenience:

Vaughan
Kitchener/Waterloo
Hamilton/Milton
Belleville/Peterborough

All routes end at Centennial Park near the town of Innisfil, ON - off highway 400, one exit south of Barrie.

Registration is only $50 per bike ($50 covers registration for both the rider and the passenger). Riders will receive a free 2013 Ride for Habitat T-shirt as well as lunch and prizes at Centennial Park.

For more information visit:  www.rideforhabitat.com

Title Sponsor - Plumbing & HVAC Magazine
Platinum Sponsor - Grundfos Canada
Silver Sponsor - Taco (Canada)

The Ride for Habitat is organized by Habitat for Humanity Canada and the HFH Huronia affiliate, with support from volunteers of the Heating, Refrigeration and Air Conditioning Institute of Canada (HRAI) and the Canadian Institute of Plumbing & Heating (CIPH).





    Facebook Twitter LinkedIn Technorati