Grundfos Case: Westin Harbour Castle & Sheraton Center Toronto

03/21/2016

Pump Audit Upgrades Deliver $120,000+ in Annual Energy Savings

“The Grundfos team was very diligent and seamlessly worked to transition the new equipment without causing any water interruption to the building.”

Yousouf J. Khan Director of Engineering – Sheraton Centre Toronto

Grundfos pump audits at the Westin Harbour Castle and Sheraton Center Toronto revealed opportunities for high efficiency, intuitive booster systems. After implementing the audit recommendations, the hotels saved a combined $120,000 in annual energy costs and moved closer to meeting their overall efficiency goals.

BoosterpaQ

BoosterpaQ


Grundfos Hydro MPC BoosterpaQ systems are made to very high standards. Thanks to the CU 352 controller, they handle even the most difficult pumping applications with ease and accuracy

Ready to Purchase

     Purchase a pump or schedule an audit/energy
     check meeting.

Ask a Question

     Ask a question or get more information about
     pump audits/energy checks.





    Facebook Twitter LinkedIn Technorati