Celebrating 50 Years of the Grundfos SP Submersible Pump

11/08/2017

We’re giving away free pump ends in celebration of the 50th anniversary of the SP submersible pump!

From November 12th through December 31st, 2017, purchase either of the following complete units for the price of just the motor.

Qualifying Models Part Number
10S05-9 (10GPM, .5 HP) 1X230V 2-WIRE 91595095
10S10-15 (10GPM, 1 HP) 1X230V 2-WIRE

91595155

Promotion Details:
Available at participating Grundfos Distributors only, you must be a water well contractor and USA resident to qualify.

Date Change: Please note, the promotion dates advertised in the November edition of Well Water Journal and National Driller were incorrect. The correct dates for
the promotion are November 12th through December 31st, 2017. We
apologize for the inconvenience.

The SP Story:
The SP was the world’s first submersible pump made entirely of stainless steel,
constructed in 1967 by Poul Due Jensen, founder of Grundfos, it quickly became
famous for its quality craftmanship - setting the standard for submersible pumps across the globe.

Since 1967, over four million SP pumps have been produced and the product
family has expanded to include 18 pump sizes ranging up to 1400 gpm and 250
hp.  With continued focus on product quality, energy efficiency, and versatility, the SP is sure to remain a contractor favorite and a cornerstone of the Grundfos pump range for years to come.

Learn more about the Grundfos SP submersible pump.