We’ll be celebrating the 50th anniversary of our SP Submersible at NGWA - visit us at booth number 301

GW-NGWA-980x150

To mark the SP’s 50th birthday we are hosting a number of special events including our first WaterPRO Championship, where well water contractors have the chance to compete and demonstrate their skills for a chance to win up to $500 in Amazon gift cards.

WaterPRO Championship
Where:
Booth number 301, during exhibit hall hours
Daily Prizes:
1st Place - $500 Amazon Gift Card
2nd Place - $300 Amazon Gift Card
3rd Place - $100 Amazon Gift Card

Take the Challenge
We’ll also be hosting a birthday party for the SP at the Stage on Broadway on Wednesday, December 6th – stop by our booth to get your wrist brand for access to our exclusive party with live music, free drinks and food.

SP Birthday Party
Visit booth number 301 during exhibition hall hours to pick up your wrist band.

SP Pump End Giveaway
From November 12th through December 31st, 2017, purchase either of the following
complete units for the price of just the motor.

Qualifying ModelsPart Number
10S05-9 (10GPM, .5 HP) 1X230V 2-WIRE91595095
10S10-15 (10GPM, 1 HP) 1X230V 2-WIRE91595155

Promotion Details
Available at participating Grundfos Distributors only, you must be a water well contractor and USA resident to qualify.