Awareness of energy efficiency in the U.S.A

01/15/2010

Two events were recently held in Washington D.C. that showed that there is an interest in reducing energy consumption in the U.S.

Grundfos is very positive about the steps that the U.S. Government and the private sector are beginning to take in overcoming the barriers to reduce energy consumption in commercial buildings.

While federal buildings use 27% less energy than 25 years ago, we must change our behaviour in combination with the new technologies that are being implemented.

More information on: www.grundfos.com/cbs